Logo
Smart Heating by Danfoss

Home heating of tomorrow

Danfoss Link™ enables you to control your home heating from anywhere. Danfoss Link™  is the only system that effortlessly lets you control both electronic radiator thermostats and floor heating.

24/7 home heating control from anywhere with the Danfoss Link™ App.

 

hand hand
Close

Danfoss Link™

Home heating of tomorrow – simple, efficient and remote

Watch video
Have a sneakpeak of our App by clicking the smartphone screen. For the full smartphone App experience, please download the App.

Your everyday life has a rhythm,
your indoor climate should, too.

 

circle

 

Leaving home

Time for 17°C

Playtime

Comfort mode: On

Bedtime

Saving mode: On

Vacation

Vacation mode: On

Calculate your savings

After

lc

Add Connect Thermostat

Savings

Up to 23% energy savings can easily be achieved *

* The calculation is based on the potential for an average German house. Therefore, it does not take variations in the individual home's insulation, building materials, windows or age into account. In addition, the calculation takes no account of external factors such as outside temperature, the use of wood-burning stove, wind force, etc. 

What people say about Danfoss Link™?

"It’s extremely precise, right down to half a degree, and gives us exceptionally good comfort. Three clicks are all it takes to tell the system when we are going out and when we are coming back."
thumb Kurt Aarhus, Denmark
"Controlling the temperature throughout the building with its 13 radiators was a hassle. Our home was either too cold when we returned home, or the system was running at full power with nobody there to enjoy the warmth."
thumb Raimund Duisburg, Germany
"I can always rely upon the temperature to be right. If I want 21°C, I’ll get it. At the same time, the Danfoss Link system has helped us reduce our energy consumption considerably."
thumb Bettina Mannheim, Germany
"The Danfoss Link system allows us to adjust room temperatures individually or group some rooms into a living zone. We can also program heating times for weekdays or weekends to match our lifestyle."
Maria Mühlheim, Germany

You typically save 5% energy every time you reduce the temperature by 1°C

Calculate the cost for equipping your home with Danfoss Link™ smart heating

How many radiators do you have?

- +

How many rooms with hydronic floor heating do you have?

- +

How many rooms with electrical floor heating do you have?

- +

Please enter at least one value

Get pricing

Danfoss recommends these products

thermo
Central Controller x1
thermo
connect™ x9
thermo
Hydronic Controller x9
ft
Floor Thermostat x9
ft
Room Sensor x9

Starting from

450 eur* *Final calculation will be done by our professional partner. Find nearest one in the map below.

Get a quote

Get a quote






Find the nearest installer

Our partners are ready to assist you.

Choose your country to find installer
Follow Linguide Danfoss

Follow the Quick start guide for setting up Danfoss Link™ – our online guide is available on your smartphone or tablet and guides you through the entire process.

Go to guide

Upgrade Central Controller via Wi-Fi

If your Danfoss Link™ Central Controller is connected to Wi-Fi, it is set to do software updates automatically.

The latest software is version 4.0.54
If your Danfoss Link™ Central Controller does not have Wi-Fi, you can update the software via USB / SD card, depending on the specific Central Controller.

Upgrade Central Controller with USB stick



First follow the link to identify, if your Central Controller with USB stick is enabled for Wi-Fi or not.

Download the software to a USB by clicking the relevant link.

Then go to your Central Controller and do the following:
1. Insert USB
2. Press the screen view Start mode
3. Select “House control”
4.Select “Settings”
5. Select “Wi-Fi and apps”
6. Select “App options”
7. Select “Software update”
8. Select “Update via USB”
9. Select “Update software now”

Update Central Controller with MiniSD Card



First download the latest software to a MiniSD Card by clicking the link.
Then go to your central controller and do the following:
1. Insert the MiniSD Card
2. Remove the front cover and press the SETUP pin for 3 seconds to enter the service area
3. Select “Software”
4. Select “Software Upgrade”
5. Select “Start Upgrade”
6. Select “Upgrade Software Now”

Note: Central Controllers from before 2010 are sometimes using software version 1.x.x. In that case, you need to update your Central Controller to version 2.1.35 before updating to the latest software.

Customize your user manual

With a customized user manual you can find instructions and advice for finding the settings that fit your exact needs.
Please select the heating devices you have bought and connected to your Danfoss Link™ and get a customized user manual by clicking “Create user manual”.

Create user manual

Connect Thermostat battery insert

Demount thermostat

Mount thermostat and adapter selection

Danfoss Link™ – mobile guide

Demount old thermostat
If you have an old thermostat on your radiator, you need to dismount your old thermostats, before you can install Connect thermostat. In the video, we illustrate how to do it – depending on which thermostat you currently have.

Mount new thermostat and adapter
First, you need to identify which adapter is right for your radiator. Danfoss provides different adapters for different radiator valve types. Use the adapter selection guide by placing the different dimensions onto the valve to identify which adapter fits your valve.

select the adapter

The adapters supplied cover more than 90 per cent of all top mounted valves, both Danfoss and other brands. If none of the adapters fit onto your valve, it may be because your valve is old. In this case, we recommend that you buy a new valve.

Second, fit the correct adapter onto the valve. Insert batteries into your new Connect thermostat and screw the thermostat onto the adapter and tighten. Leave mounting mode.

Please watch the how-to videos for a full explanation.

Now you are ready to create room and add devices on your Danfoss Link™ Central Controller. Please follow linkguide.danfoss.com to do this.

 

 

Adding devices
You can add devices to your Danfoss Link™ by following the Quick start guide on linkguide.danfoss.com. Remember to keep track of the devices you have added to Danfoss Link™, so you know in which room to mount the device.

Note: If your Central Controller says that the device was not successfully added, please reset the device (watch video below).

Moving or removing devices
If you wish to remove a device or move it to another room, reset the device you wish to move or remove (watch reset device video).

The device is now ready to be re-installed. Please follow the Quick start guide on linkguide.danfoss.com.

Power outage on Danfoss Link™ Central Controller
If there is a power outage, the Danfoss Link™ Central Controller will turn on, once it gets power again and will connect to your installed devices.
If the Central Controller does not get power again

  • Connect thermostats will continue on the temperature they were at when the power outage happened
  • the Room Sensor will go into frost protection mode

Connect or Room Sensor runs out of battery
When Connect or Room Sensor is low on a battery, a battery icon will shown in the display and the Central Controller will give you an error message. If a Connect thermostat or Room Sensors runs out of battery, they will go into frost protection mode.
Connect thermostats and Room Sensors use 2 x AA non-rechargeable batteries each.

The freer passage the radio signal from the Central Controller has, the farther it can reach. House walls, metal objects, special constructions and other obstacles weaken the signal. Your Central Controller will give an alarm if it cannot reach a device for more than 1.5 hours.

central controller connection 1 central controller connection 2

If there are obstacles between your devices, you may need to install a Repeater Unit to extend the signal. Follow linkguide.danfoss.com to install the device. If necessary, you can extend the extended signal by adding another Repeater Unit as illustrated below. You only need one Central Controller for your home.

central controller connection 3

It can measure and control the temperature at a specific spot in your home.

If you place the Room Sensor close to your couch or away from a window, you ensure your desired temperature at this spot, because you optimize the actual temperature measurement in the room.

We recommend adding a Room Sensor in rooms with multiple radiators, because the Room Sensor balances the temperature across radiators based on the room temperature.

If your radiator thermostat is covered, e.g. by furniture, the Room Sensor will ensure your desired temperature in the room.

Add the Room Sensor to your Danfoss Link™ Central Controller in the same room as the Connect Thermostat you want the Room Sensor to be connected to.

room-sensor-2

 

Energy savings are achieved through a reduction in room temperature.

Energy efficiencyAs a general rule, you can save 5% of energy consumption for every degree you lower the temperature at night. We recommend, you lower the temperature 3-4 °C at night and during working hours, e.g. from 21°C to 17°C. Also, activate vacation mode when you are on holiday.
When using Connect Thermostat, the average European saving potential is up to 30% on your heat consumption. Read more here.

The older your thermostats are when exchanging them, the greater your energy savings will be.

Connect Thermostat was the first electronic thermostat ever to achieve the prestigious AA energy certificate from eu.bac.

To ensure that the radiator thermostat can reach the set temperature quickly, we recommend a difference between Away/Asleep mode and At Home mode at max. 4 ˚C.

Danfoss Link™ offers a precise and energy efficient heating regulation by adapting itself to the heating system. This takes approximately one week after installation. Therefore, during the first week you can experience fluctuations as the thermostats are learning when to start heating to reach the specific temperature at the specific time (adaptive learning). After this period, you can enjoy the perfect temperature in your home whenever you want it.

Below is an illustration of which Danfoss Link™ products are room devices and which are service devices.

The Danfoss Link™ Central Controller can be used in detached single-family homes of less than 300 m² with a maximum of 30 Connect Thermostats per Danfoss Link™ Central Controller.

smart heating for all types of buildings

You can connect up to 50 devices in total to Danfoss Link™ Central Controller and thereof max. 30 Connect Thermostats to  Danfoss Link™. Danfoss Link™ controls up to 10 devices in one room.
Maximum number of devices you can add to Danfoss Link™:

 

How many devices with Danfoss link Central Controller

Yes, if you have the Wi-Fi version of Danfoss Link™ Central Controller. You can download the app from either App Store or Google Play.

Find out if your Danfoss Link™ supports Wi-Fi here.

appstore googleplay

No. Danfoss Link™ assigns a unique ID to every device in the network, so your neighbour cannot control your devices via his Controller. To ensure reliable wireless communication, Danfoss Link™ uses a robust and world-leading communication technology that is designed specifically for control applications in houses, apartments and smaller offices.

No. Eco™ is a stand-alone product. You need to use Connect Thermostat for Danfoss Link™.

Danfoss ensures that all the devices in your home and the cloud service we provide to your smartphone are secure at all times. The Danfoss Link™ App is developed on a Home Banking platform and so the pairing of the Danfoss Link™ App to the Danfoss Link™ Central Controller is fully secure.

Read End User License Agreement and Disclaimer here.

Contact us

Please write a message or call us on phone +45 7488 2222.

Contact us

Are you:  Consumer Professional




I already have Danfoss Link™ at home:  YES NO

Help us improve and share your experience on Danfoss Link™




By submitting, you agree that Danfoss can contact you on above phone and/or email for feedback and research purposes.